Skip to content
<< Back
Feb 14, 2018

CommScope Enters Fixed Wireless Market with Open Interface, Integrated Antenna Solution

HICKORY, N.C. --(BUSINESS WIRE)-- CommScope is joining the fixed wireless access market with the introduction of a new integrated antenna solution based on xRAN open interface specifications. The open interface allows wireless operators to mix and match radio access network (RAN) hardware from

HICKORY, N.C.--(BUSINESS WIRE)-- CommScope is joining the fixed wireless access market with the introduction of a new integrated antenna solution based on xRAN open interface specifications. The open interface allows wireless operators to mix and match radio access network (RAN) hardware from multiple vendors to more flexibly address varying requirements.

This press release features multimedia. View the full release here: http://www.businesswire.com/news/home/20180214005374/en/

CommScope has developed a 5G radio/antenna solution that supports millimeter-wave spectrum and works ...

CommScope has developed a 5G radio/antenna solution that supports millimeter-wave spectrum and works on a completely virtualized baseband with an open interface for fixed wireless access. (Photo: Business Wire)

CommScope has developed an attractive 5G radio/antenna solution that supports millimeter-wave spectrum and works on a completely virtualized baseband with an open interface. This solution integrates a beamforming active antenna array operating at 28 GHz and will be available for trial with a third-party baseband platform to create a high performance and highly flexible 5G access network.

"Our integrated antenna will enable the full capabilities of 5G millimeter-wave spectrum bands while offering maximum flexibility in an evolving air-interface environment," said Farid Firouzbakht, senior vice president, RF Products, CommScope. "As a contributing member to the xRAN organization, we endorse the benefits of an open baseband interface for enabling more innovation in the wireless marketplace."

Fixed wireless access is a method for delivering broadband internet access, voice and video services to homes or businesses without a wired connection, and is one of the first 5G use cases. With CommScope's new solution, wireless operators can use commercial off-the-shelf servers to trial virtualized network functions for fixed wireless access applications. The new CommScope solution includes:

  • A base station antenna with full 120-degree beam-steering of four independent MIMO (multiple input/multiple output) ports, using a CommScope patented 256-element antenna array.
  • An integrated remote radio unit with industry-leading effective isotropic radiated power (EIRP) in a compact enclosure of less than 10 liters volume, passively cooled and optimized to fit within concealment solutions.

CommScope has also developed a sophisticated testing facility for the development of 5G related millimeter antenna technology. Located near Dallas, Texas, this automated far field anechoic testing chamber is capable of completely automated millimeter wave beamforming calibration and ready for trials of 5G massive MIMO systems.

CommScope will make its integrated 5G radio/antenna solution available for trials in mid-2018. The company will highlight it at Mobile World Congress 2018 in Hall 2, stand 2J30.

About CommScope:

CommScope (NASDAQ: COMM) helps design, build and manage wired and wireless networks around the world. As a communications infrastructure leader, we shape the always-on networks of tomorrow. For more than 40 years, our global team of greater than 20,000 employees, innovators and technologists have empowered customers in all regions of the world to anticipate what's next and push the boundaries of what's possible. Discover more at http://www.commscope.com.

Follow us on Twitter and LinkedIn and like us on Facebook.

Sign up for our press releases and blog posts.

This press release includes forward-looking statements that are based on information currently available to management, management's beliefs, as well as on a number of assumptions concerning future events. Forward-looking statements are not a guarantee of performance and are subject to a number of uncertainties and other factors, which could cause the actual results to differ materially from those currently expected. In providing forward-looking statements, the company does not intend, and is not undertaking any obligation or duty, to update these statements as a result of new information, future events or otherwise.

News Media Contact:
Bill Walter, CommScope
+1 708-236-6634
publicrelations@commscope.com
or
Financial Contact:
Jennifer Crawford, CommScope
+1 828-323-4970

Source: CommScope

News Provided by Acquire Media