Adding Cells Is a Small Antenna Matter for CommScope
—Small Antenna Technology Is Critical to Cell Densification—

An Andrew Metro Cell sector antenna mounted to a street pole uses significant beam management tools to reduce cell to cell interference and optimize capacity. (Photo: Business Wire)
Network operators use multiple frequency
bands and multiple air-interface
technologies to meet subscriber demand, which typically means larger
antennas. CommScope's small antenna technology enables physically
smaller base station antennas to handle these requirements while
offering superior performance.
For macro cell sites:
-
Increasing sector capacity by adding new RF signals without losing
power or control has often increased the antenna's width. While this
solves the RF challenge well, it adds weight, increases wind load and
may even complicate zoning. To solve this challenge,
CommScope is working on a new line of antennas that provide eight or more ports with little to no change in the overall dimensions, meaning no extra leasing costs. This antenna is intended for adding more sectors and capacity on towers and other macro sites.
For smaller cell sites, which are critical to network densification:
- The Micro AcCELLerator™ is a tri-sector concealment solution for tough zoning areas. This antenna platform packs a full cell site of capacity and coverage into a small diameter antenna body that better fits strict cell site zoning requirements. A typical deployment scenario is a congested urban area lacking usable tower space but with a high concentration of users that need more capacity. One recently released platform provides a full cell site covering 1710-2690 MHz with dual polarized antennas equipped with remote beam tilting capability in a diameter of only 200 millimeter wide, easily concealable in a flag pole or street lamp.
- The Metro Cell Antenna platform is defined by antennas specifically aimed at physical size limitations of up to one meter in height. This family includes a recently released quasi-omni antenna and sector antenna that allow the network designer to use significant beam management tools that reduce cell to cell interference and optimize capacity. By using this more sophisticated antenna solution, studies have shown that the number of "small cells" needed in a high traffic area could be reduced by as much as 25 percent.
"Wireless networks need lots of options to drive additional capacity via
overall network densification, and small antenna technology will play a
major role in that area," said
To learn more about Andrew small antenna technology, schedule
a meeting with
Related Blog Posts:
How to Efficiently Support Multiple Frequency Bands
Coming Soon! Antenna Evolution Focus Day
The Difference between 3G and 4G
Andrew is a registered trademark of
About
This press release includes forward-looking statements that are based on information currently available to management, management's beliefs, as well as on a number of assumptions concerning future events. Forward-looking statements are not a guarantee of performance and are subject to a number of uncertainties and other factors, which could cause the actual results to differ materially from those currently expected. In providing forward-looking statements, the company does not intend, and is not undertaking any obligation or duty, to update these statements as a result of new information, future events or otherwise.
Photos/Multimedia Gallery Available: http://www.businesswire.com/multimedia/home/20140902005210/en/
News Media Contact:
+1
708-236-6634 or publicrelations@commscope.com
or
Financial
Contact:
+1 828-323-4848
Source:
News Provided by Acquire Media