Another CommScope Breakthrough for the Cellular Network— Plug-and-Play at the Top of the Tower
—Latest Tower Top Innovation Aims for Further Simplicity, and Time and Cost Savings for Operators—

Andrew SiteRise Standard Interface simplifies the interface between the base station antenna and virtually any remote radio unit, making it easier to do field replacements and upgrades. (Photo: Business Wire)
Andrew SiteRise, unveiled in 2013, is the world's first pre-assembled tower top solution, designed to bring factory assembled quality and consistency to the field assembly environment of a wireless network cell site. Andrew SiteRise facilitates the rapid implementation of RRU technology in close physical proximity to the antenna connectors, reducing losses and improving network performance. The SiteRise solution already is proving cost-effective for operators by moving the complex connection, configuration and testing work from the top of the tower to ground level where it can be done in a controlled environment.
"Since we began implementing the SiteRise solution in close
collaboration with a major wireless operator, we have continued to work
closely with the whole operator community to understand what innovations
would be of additional value to them," said
SiteRise Standard Interface is a new way of connecting an RRU to the base station antenna, using a unique approach not previously utilized for tower top applications. SiteRise Standard Interface gives an operator the flexibility of using multiple RRU technologies and frequency bands in a simplified plug-and-play arrangement. Key to this solution is a patented connector technology that provides an essentially passive intermodulation (PIM)-free, blind mate connection.
SiteRise Standard Interface offers lower risk and higher quality assurance by moving the complex connecting work at the top of the tower into a more controlled environment. This innovation reduces the risk of craft related errors due to the harsher and more complex working conditions at the top of the tower. The easy accessibility enabled by SiteRise Standard Interface makes upgrading RRUs for changing frequency and technology requirements a plug-and-play feature. Ultimately, SiteRise Standard Interface reduces the time installers spend working on the tower, saving operating costs and creating faster site turn ups, critical for operators' time-to-market competitive advantage.
"Our antenna/RRU SiteRise Standard Interface combines the best features of putting remote radios close to the antenna for reducing signal loss and energy consumption, but maintains a level of independence between the radio and antenna for flexibility and ease of support," said Cardwell.
SiteRise Standard Interface introduces a new connector technology that provides an essentially PIM-free, blind mate connection. PIM is a major concern with today's interference limited technologies such as LTE. With blind mate connection capability, upgrading and maintaining radio technology can be done without affecting the antenna's position. This functionality reduces the time and cost associated with radio maintenance, and, even more importantly, reduces the risks associated with technology obsolescence.
Combining multiple frequencies is also common in today's cell sites. SiteRise Standard Interface includes an optional filter integration that reduces potential sources of interference and the need for more complex solutions internal to the RRU technology.
As part of its evolution of solutions at the top of the tower,
"The top of the tower is a difficult place to work, so having a solution
that provides for a more consistent and predictable quality result and
provides flexibility for change just makes sense," said
The latest evolution of CommScope's Andrew SiteRise solution will be
introduced at
Related Blog Posts:
Bringing Fiber to the Antenna - What's Your Strategy?
How to Make a Standardized Tower Top
How
to Implement LTE in
Andrew, HELIAX, and FiberFeed are registered trademarks of
About
This press release includes forward-looking statements that are based on information currently available to management, management's beliefs, as well as on a number of assumptions concerning future events. Forward-looking statements are not a guarantee of performance and are subject to a number of uncertainties and other factors, which could cause the actual results to differ materially from those currently expected. In providing forward-looking statements, the company does not intend, and is not undertaking any obligation or duty, to update these statements as a result of new information, future events or otherwise.
Photos/Multimedia Gallery Available: http://www.businesswire.com/multimedia/home/20140212005084/en/
News Media Contact:
publicrelations@commscope.com
or
Financial
Contact:
Source:
News Provided by Acquire Media