CommScope Extends Next Generation Fiber Frame Portfolio
—New Frame, Enhanced High-Density Fiber Blocks Provide Seamless Expansion for Higher Bandwidth Needs—
This Smart News Release features multimedia. View the full release here: http://www.businesswire.com/news/home/20151209005114/en/
The new frame is seven feet tall and 24 inches deep and can be installed directly next to existing traditional 30-inch wide NGF frames. The pre-terminated fiber blocks eliminate the need to individually plug in hundreds of connectors at the rear of the panel, thus replacing a large number of installation steps. Installers plug pre-terminated MPO assemblies directly into modules at the rear, which distribute trunk fibers into 10G or 40G channels at the front. All pre-populated blocks are factory tested, assembled, and packaged to provide maximum craft friendliness. Pre-terminated blocks with cable stubs are also available.
"Network managers need rapid deployment and space efficiency to cope
with the accelerated need for bandwidth due to increased mobile traffic,
big data demands, and other factors," said
The Enhanced High Density NGF and pre-loaded fiber blocks support rapid and cost-effective deployment with the following features:
- Exceptional fiber density with improved front and rear connector access, simplified patching and ample cable management provisions
- Blocks are available in 288 count, LC-MPO and 288 count LC-stub versions.
- Single mode blocks are available in 10, 40 and 100 G formats
- Assured performance - Each module is pre-tested in the factory, and test data is traceable via a bar code to a test database
- Packaging protects the connectorized blocks and speeds "bolt-in" installation
- Modules are clearly marked for simplified labeling and documentation
To learn out more about the Next Generation Fiber Frame, download the product catalog here.
About
Follow us on Twitter and LinkedIn and like us on Facebook.
Sign up for our press releases and blog posts.
This press release includes forward-looking statements that are based on information currently available to management, management's beliefs, as well as on a number of assumptions concerning future events. Forward-looking statements are not a guarantee of performance and are subject to a number of uncertainties and other factors, which could cause the actual results to differ materially from those currently expected. In providing forward-looking statements, the company does not intend, and is not undertaking any obligation or duty, to update these statements as a result of new information, future events or otherwise.
View source version on businesswire.com: http://www.businesswire.com/news/home/20151209005114/en/
News Media Contact:
+1 972-804-2954 or publicrelations@commscope.com
or
Financial
Contact:
+1 828-323-4970
Source:
News Provided by Acquire Media