CommScope Launches SYSTIMAX Constellation Enterprise Power and Data Platform for the Hyperconnected Future
Modular platform allows enterprises to build scalable 10G and fault-managed power networks incrementally with minimal cost, space, labor, and time
Compared to traditional structured cabling networks, the Constellation platform utilizes a radically simplified architecture that is both modular and technology-agnostic. This allows it to use fewer components while supporting both converged and segmented networks, AC and DC power applications and a variety of connectivity standards. As a result, the Constellation platform delivers greater power and faster speeds to more devices, requiring less space and lowering the overall carbon footprint of the network. It is an unparalleled solution for quickly and efficiently deploying the next generation of enterprise edge networks.
The system leverages fault-managed power, which safely transmits more power over less copper than traditional powering technologies. That approach, deployed in a star network topology, extends service distances from equipment rooms and delivers 10G speeds and 1kW power to a growing number of connected devices in increasingly dense urban environments.
The Constellation platform uses a distributed star topology to extend services from equipment rooms to a service area or zone to support proximate devices. Its simplified architecture can significantly reduce the copper and plastic in the network, in some cases by nearly 60%, and the typical installation can reduce labor hours by over 50% over traditional systems.
“The Constellation platform addresses our customers’ growing need to build and augment IP networks in response to the densification of urban centers and the proliferation of connected devices,” stated
About Constellation
This platform is part of CommScope’s award-winning SYSTIMAX cabling and connectivity solutions. The platform consists of Propel™ fiber panels, power transmitters and power transition panels, which connect to ceiling-mounted Constellation Points via patented hybrid power/data fiber trunks, and finally to devices using pre-terminated SYSTIMAX Cat 6A patch cords and cable assemblies.
By the numbers, the Constellation platform delivers up to:
1000W power supply (across 110V AC, 48V and 24V DC systems and PoE)
500M effective transmission distance between equipment room and convergence points
10G bandwidth capabilities
57% reduction in skilled labor hours required to install
50 devices supported per Constellation convergence point
The Constellation platform is available immediately in
About
Follow us on Twitter and LinkedIn and like us on Facebook.
Sign up for our press releases and blog posts.
This press release includes forward-looking statements that are based on information currently available to management, management’s beliefs, as well as on a number of assumptions concerning future events. Forward-looking statements are not a guarantee of performance and are subject to a number of uncertainties and other factors, which could cause the actual results to differ materially from those currently expected. In providing forward-looking statements, the company does not intend, and is not undertaking any obligation or duty, to update these statements as a result of new information, future events or otherwise.
Source:
View source version on businesswire.com: https://www.businesswire.com/news/home/20230810782316/en/
News Media Contact:
Luke.Hamer@commscope.com
Financial Contact:
+1 630-281-3413
Source: