CommScope Partners with Hydrogenics to Provide Indoor Backup Power Solution for Data Centers
-Data center operators benefit from a clean backup power solution that occupies the same space as one server cabinet -

Hydrogen Fuel Cell Rack In
Believed to be the first-of-its-kind, this scalable indoor fuel cell
solution can provide up to 30 kilowatts (kW) of reliable,
environmentally-friendly backup power to enterprise computing systems.
This is enabled through an existing partnership with
"Power loss can affect lines of businesses and impact the ability to
maintain service level performance with customers," said
Multiple power racks can be installed to scale in 30kW increments and sustain a variable runtime from hours to days, based on customer requirements and hydrogen tank options. With the width of a standard server cabinet and the height of only six-and-a-half feet, the cabinet can easily fit at the end of a data center row without taking up a large amount of valuable real estate.
"Space within most data centers is at a premium and this backup power
solution takes up the least amount compared to a battery rack or other
backup power solutions," said
When paired with an appropriate uninterruptable power supply, the scalable indoor fuel cell rack can be configured for 10, 20 or 30kWs of sustained alternating current power. The fuel cell solution is quiet, emits no greenhouse gases and can be deployed indoors with the hydrogen fuel tank sited outside the building. These racks are an ecological alternative to battery racks and generators.
The fuel cell solution converts chemical energy directly into electrical energy without any combustion. The system provides highly efficient, reliable and uninterrupted backup power to data center and business systems without the need for costly regular maintenance. The only by-products are heat and a small amount of water.
For more information on CommScope's indoor fuel cell solution, visit: http://www.commscope.com/Solutions/Enterprise-Solutions/Intelligent-Building-Solutions/Business-Continuity-Solutions/
Related Blog Posts:
Critical Facilities Are Critical—Let's Be Prepared
Say
No to Inefficient, Energy-Wasting,
Bringing Technology, Intelligence and Energy to Bear—A Vision for Sustainable Critical
Hydrogen Safety and Standards - The FUD Cloud
Fuel Cell Makes Impact at SCTE's Green Pavillion
About
About
This press release includes forward-looking statements that are based on information currently available to management, management's beliefs, as well as on a number of assumptions concerning future events. Forward-looking statements are not a guarantee of performance and are subject to a number of uncertainties and other factors, which could cause the actual results to differ materially from those currently expected. In providing forward-looking statements, the company does not intend, and is not undertaking any obligation or duty, to update these statements as a result of new information, future events or otherwise.
Photos/Multimedia Gallery Available: http://www.businesswire.com/multimedia/home/20140610005362/en/
News Media Contact:
+1
972-952-9780
publicrelations@commscope.com
or
Financial
Contact:
+1 828-323-4848
or
+1 646-438-9385
cwitty@darrowir.com
Source:
News Provided by Acquire Media