CommScope Revolutionizes Wireless Network Testing with Groundbreaking PIM Solution
A single technician can connect directly to the base band unit at the bottom of the tower with the Optical PIM Tester. (Photo: Business Wire)
A revolutionary test methodology is introduced with the affordable, portable tester. For the first time ever, a single technician can connect directly to the base band unit at the bottom of the tower and perform a "truly active" PIM test over the Common Public Radio Interface (CPRI) by using the Optical PIM Tester.
Additionally, the Optical PIM Tester can easily be included within every technician's arsenal thanks to its compact size and ease of use. It provides a convenient, user-friendly interface that is accessible from a smartphone, tablet or notebook computer. Entire technical crews including tower climbers no longer need to be sent out to a site to test for PIM by disconnecting coaxial cable from antennas, potentially introducing new PIM in the test process.
"As PIM requirements become more stringent as demanded by LTE networks,
it gets harder to determine if there is a PIM problem needing
remediation," said
The Optical PIM Tester features:
- Active PIM testing over CPRI by injecting signals into the downlink and looking for PIM products in the uplink, making it easier to identify
- Support for all frequency bands in one unit, eliminating the need for multiple PIM units
- Simultaneous access to multiple sectors and frequency bands, saving on testing time
- PIM testing at ground level, increasing safety and massively reducing costs and time
- A user-friendly interface that is accessible from a smartphone, tablet or notebook computer
Part of the Andrew Solutions® portfolio, the Optical PIM Tester is a battery powered, ruggedized, portable unit that connects between the base band unit and remote radio units using fiber optic cables. The Optical PIM Tester enables a single technician to test for PIM in a fraction of the time required with legacy PIM testers. When a smartphone, tablet or a notebook computer connects to the Optical PIM Tester over Wi-Fi, a user-friendly interface appears for executing the test process. The system is highly automated, requiring no specialized knowledge of PIM.
"The intense scrutiny of PIM is not going away, and we envision a resource like our Optical PIM Tester will become a fundamental part of every operator's effort to minimize PIM," said Kurk. "CommScope is helping operators manage PIM before it degrades their networks."
PIM is interference resulting from the mixing of two or more frequencies in a passive circuit. If the interference coincides with a network's transmit frequencies, it can cripple network performance and throughput. PIM can occur from a loose or poorly made cabling connection, an incorrectly torqued connector or a poorly manufactured or installed antenna, filter, or remote radio head—and can degrade the network dramatically. For example, just a one decibel drop in uplink sensitivity due to PIM can reduce wireless coverage in an LTE network by 11 percent.
Related Blog Posts:
The Importance of PIM - and How to Safeguard Your Network Against It
PIM Requirements Must Increase to Support Evolving DAS Systems
Andrew Solutions is a registered trademark of
About
Follow us on Twitter and LinkedIn and like us on Facebook.
Sign up for our press releases and blog posts.
This press release includes forward-looking statements that are based on information currently available to management, management's beliefs, as well as on a number of assumptions concerning future events. Forward-looking statements are not a guarantee of performance and are subject to a number of uncertainties and other factors, which could cause the actual results to differ materially from those currently expected. In providing forward-looking statements, the company does not intend, and is not undertaking any obligation or duty, to update these statements as a result of new information, future events or otherwise.
Photos/Multimedia Gallery Available: http://www.businesswire.com/multimedia/home/20150224005195/en/
News Media Contact:
+1
708-236-6634
publicrelations@commscope.com
or
Financial
Contact:
+1 828-323-4848
Source:
News Provided by Acquire Media